The PM_Sensorless project in ControlSuite generates a build error when imported and built in CCS 6.1.1.
The version of ControlSuite is v3.3.4 and the project is the one in C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\PM_Sensorless.
Importing this project into CCS 6.1.1 and building the F2803x_RAM configuration results in this error:
error: file
"C:/ti/controlSUITE/libs/math/FPUfastRTS/V100/lib/rts2800_fpu32_fast_supplement.lib<div_f32.obj>"
specifies ISA revision "C28FPU32", which is not
compatible with ISA revision "C2800" specified in a previous file or on the
command line
Please see this thread in the CCS forum for the original customer post:
https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/463307/1665432#1665432