This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F2837x control CARD R1.1 stuck (Trouble Halting Target CPU)

Other Parts Discussed in Thread: UNIFLASH

Hi,

I am evaluating the F2837x with the associate controlCard.

It works without any issue before I flashed a code with a CPU clk that seems to stuck the eval board.

"    InitSysPll(XTAL_OSC,IMULT_120,FMULT_1,PLLCLK_BY_40);     "

Now when I am trying to connect to the target or try to flash a new code I have the following issue:

In the pop up:

Trouble Halting Target CPU:
(Error -1156 @ 0x0)
Device may be operating in low-power mode. Do you want to bring it out of this mode?
(Emulation package 6.0.14.5)

In the Console:

C28xx_CPU1: Trouble Halting Target CPU: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
C28xx_CPU1: Error: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
C28xx_CPU1: Trouble Writing Memory Block at 0x5f432 on Page 1 of Length 0x1: (Error -2130 @ 0x800) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
C28xx_CPU1: GEL: Error while executing OnTargetConnect(): Target failed to write 0x0005F432@Data     at *((int *) 0x5F432)=0x003F [f28377d_cpu1.gel:81]     at OnTargetConnect() .
C28xx_CPU1: Failed CPU Reset: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? (Emulation package 6.0.14.5)
C28xx_CPU1: Failed Software Reset: A reset is already in progress: (Error -1138 @ 0x0) Device refused to allow debug mode. Power-cycle the board. If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)

I tried UniFlash but the target is also stuck via the other software.

Do you have any idea ?

Thanks and best regards,

Mathieu