This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377D can't allocate the SCI_A to CPU2?

GPIO/_SetupPinOptions(28, GPIO_INPUT, GPIO_PUSHPULL);

GPIO_SetupPinMux(28, GPIO_MUX_CPU2, 1);  //SCI GPIO Setup
   GPIO_SetupPinOptions(29, GPIO_OUTPUT, GPIO_ASYNC);
   GPIO_SetupPinMux(29, GPIO_MUX_CPU2, 1);
   DevCfgRegs.CPUSEL5.bit.SCI_A = 1;

I configue the IO and function of SCIA as above, but SCIA can't work in CPU2 and still can work in CPU1, what I missed?

Thanks a lot! 

  • Hi Elvis,

    Please check if you have enabled the CLOCK for SCI_A from CPU2 using PCLKCR7 register. Also the code you have given above is getting executed from CPU1. Right?

    Regards,

    Vivek Singh

  • Hi, Vivek

    If I allocate the SCIA to CPU1, the code is correct working in CPU1. And as I change to CPU2 as the code showing above ( with PCLKCR7 register set to “1” in CPU2), the SCIA still worked in CPU1 !

    Because I used EPWM also in CPU2, the EPWM can work in CPU2 correctly, so it confused me, why the SCIA can't be allocated to CPU2 and still working in CPU1?

  • Elvis,

    If there is no issue with sharing the code, please attach CPU1/CPU2 code you are using in this case.

    Regards,

    Vivek Singh

  • CPU1

    #include "F28x_Project.h"
    #include "F2837xD_Ipc_drivers.h"
    #include "RS232.h"
    Uint16 Reciever2;

    void main(void)
    {
    InitSysCtrl();

    #ifdef _STANDALONE
    #ifdef _FLASH
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH);
    #else
    IPCBootCPU2(C1C2_BROM_BOOTMODE_BOOT_FROM_RAM);
    #endif
    #endif

    #ifdef _FLASH
    InitFlash();
    #endif

    InitGpio(); // Skipped for this example
    EALLOW;
    GpioCtrlRegs.GPADIR.bit.GPIO13= 1
    GPIO_SetupPinOptions(14, GPIO_OUTPUT, GPIO_PUSHPULL);
    GPIO_SetupPinMux(14, GPIO_MUX_CPU2, 4);
    GPIO_SetupPinOptions(28, GPIO_INPUT, GPIO_PUSHPULL);
    GPIO_SetupPinMux(28, GPIO_MUX_CPU2, 1); //SCI GPIO Setup
    GPIO_SetupPinOptions(29, GPIO_OUTPUT, GPIO_ASYNC);
    GPIO_SetupPinMux(29, GPIO_MUX_CPU2, 1);
    DevCfgRegs.CPUSEL5.bit.SCI_A = 1;
    //TODO Add code to allow configuration of GPADIR from CPU02 using IPC
    EDIS;
    GpioDataRegs.GPADAT.bit.GPIO13 = 1;

    DINT;


    InitPieCtrl();

    // scia_fifo_init(); // Initialize the SCI FIFO
    // scia_echoback_init(); // Initialize SCI for echoback


    IER = 0x0000;
    IFR = 0x0000;


    InitPieVectTable();

    EINT;
    ERTM;

    for(;;)
    {
    GpioDataRegs.GPADAT.bit.GPIO13 = 0;
    GPIO_WritePin(14, 1);
    // scia_msg("Hello World!:\0");
    // SciRecieve(&Reciever2);
    DELAY_US(1000 * 500);

    GpioDataRegs.GPADAT.bit.GPIO13 = 1;
    GPIO_WritePin(14, 0);

    DELAY_US(1000 * 500);
    }
    }
  • CPU2


    Uint16 Reciever2;
    void main(void)
    {
    #ifdef _FLASH
    memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
    #endif
    InitSysCtrl();

    #ifdef _FLASH
    InitFlash();
    #endif

    EALLOW;
    CpuSysRegs.PCLKCR7.bit.SCI_A = 1;
    EDIS;
    GPIO_WritePin(14, 1);
    DINT;

    InitPieCtrl();
    EALLOW;
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
    EALLOW;
    scia_fifo_init(); // Initialize the SCI FIFO
    scia_echoback_init(); // Initialize SCI for echoback
    CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1;
    EDIS;

    IER = 0x0000;
    IFR = 0x0000;

    InitPieVectTable();

    EINT;
    ERTM;

    for(;;)
    {
    //
    //
    GPIO_WritePin(14, 0);
    scia_msg("Hello World!:\0");
    SciRecieve(&Reciever2);
    //
    //
    DELAY_US(1000 * 250);

    //
    //
    GPIO_WritePin(14, 1);
    //
    //
    DELAY_US(1000 * 250);
    }
    }
  • RS232.c


    #include "RS232.h"
    #include "F28x_Project.h"
    #include <stdlib.h>

    char* SendMessage;
    char RecieveData[10];
    Uint16 Reciever;
    Uint32 out;

    void scia_echoback_init()
    {
    // Note: Clocks were turned on to the SCIA peripheral
    // in the InitSysCtrl() function

    SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
    // No parity,8 char bits,
    // async mode, idle-line protocol
    SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
    // Disable RX ERR, SLEEP, TXWAKE
    SciaRegs.SCICTL2.all =0x0003;
    SciaRegs.SCICTL2.bit.TXINTENA =1;
    SciaRegs.SCICTL2.bit.RXBKINTENA =1;

    //
    // SCIA at 9600 baud
    // @LSPCLK = 50 MHz (200 MHz SYSCLK) HBAUD = 0x02 and LBAUD = 0x8B.
    // @LSPCLK = 30 MHz (120 MHz SYSCLK) HBAUD = 0x01 and LBAUD = 0x86.
    //
    SciaRegs.SCIHBAUD.all =0x0002;
    SciaRegs.SCILBAUD.all =0x008B;

    SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
    }
    void scia_xmit(int a)
    {
    while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {}
    SciaRegs.SCITXBUF.all =a;
    }

    void scia_msg(char * msg)
    {
    int i;
    i = 0;
    while(msg[i] != '\0')
    {
    scia_xmit(msg[i]);
    i++;
    }
    }

    // Initialize the SCI FIFO
    void scia_fifo_init()
    {
    SciaRegs.SCIFFTX.all=0xE040;
    SciaRegs.SCIFFRX.all=0x204f;
    SciaRegs.SCIFFCT.all=0x0;
    }

    unsigned int SciRecieve(unsigned int *a)
    {
    unsigned int x;
    x=0;

    if(SciaRegs.SCIFFRX.bit.RXFFST!=0)
    {
    Reciever=SciaRegs.SCIFFRX.bit.RXFFST;
    for(out=0; out<Reciever; out++)
    {
    RecieveData[out]= SciaRegs.SCIRXBUF.all;
    }
    *a=atol(RecieveData);
    x=1;
    }
    return x;
    }

    void SciTran(unsigned int a)
    {
    Uint16 i;
    i=0;
    ltoa(a, SendMessage);
    *SendMessage+='\0';
    while(SendMessage[i] != '\0')
    {
    scia_xmit(SendMessage[i]);
    i++;
    }

    }
  • RS232.h

    extern void scia_echoback_init(void);
    extern void scia_fifo_init(void);
    extern void scia_xmit(int a);
    extern void scia_msg(char *msg);
    extern unsigned int SciRecieve(unsigned int *a);
    extern void SciTran(unsigned int a);

    extern char* RS232_Transmit;
    extern char* RS232_Recieve;


    extern char* SendMessage;
    extern char RecieveData[10];
  • RS232.h

    extern void scia_echoback_init(void);
    extern void scia_fifo_init(void);
    extern void scia_xmit(int a);
    extern void scia_msg(char *msg);
    extern unsigned int SciRecieve(unsigned int *a);
    extern void SciTran(unsigned int a);

    extern char* RS232_Transmit;
    extern char* RS232_Recieve;


    extern char* SendMessage;
    extern char RecieveData[10];
  • Hi Chen,

    Sorry for late reply.

    I see following line in CPU1 code which has issue.

    GPIO_SetupPinMux(29, GPIO_MUX_CPU2, 1);
    DevCfgRegs.CPUSEL5.bit.SCI_A = 1;

    If you look at the GPIO_SetupPinMux() function, it has EDIS instruction at the end of the function which means "DevCfgRegs.CPUSEL5.bit.SCI_A = 1;" code does not have EALLOW enable hence this write will not go through.

    Please change this code like below -

    GPIO_SetupPinMux(29, GPIO_MUX_CPU2, 1);

    EALLOW;
    DevCfgRegs.CPUSEL5.bit.SCI_A = 1;

     

    Hope this fixes the issue.

     

    Regards,

    Vivek Singh

  • Yes, Thank you Vivek.