I have a current controller working quite good using lab4. The low load rpm is 1800. I wish the rpms were closer to 5000, which is the rating of the motor. How can the rpm be adjusted up without changing the current set point? This is a 12 pole bldc motor.
Thank you!