Hi all,
I am using adc_soc program with slight modification. My program is given below. The problem is when I give input to ADCIN0 I get a digitalised waveform. When the same input is given to ADCIN1 I am getting highly distorted waveform. I tried changing ADCINx to many other pins. But second Channel always provides high noise.
The program is written below:
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
// Prototype statements for functions found within this file.
interrupt void adc_isr(void);
// Global variables used in this example:
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Voltage1[1500];
Uint16 Voltage2[1500];
main()
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the DSP2833x_SysCtrl.c file.
 InitSysCtrl();
EALLOW;
 #if (CPU_FRQ_150MHZ) // Default - 150 MHz SYSCLKOUT
 #define ADC_MODCLK 0x3 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 150/(2*3) = 25.0 MHz
 #endif
 #if (CPU_FRQ_100MHZ)
 #define ADC_MODCLK 0x2 // HSPCLK = SYSCLKOUT/2*ADC_MODCLK2 = 100/(2*2) = 25.0 MHz
 #endif
 EDIS;
// Step 2. Initialize GPIO:
// This example function is found in the DSP2833x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
 DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2833x_PieCtrl.c file.
 InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
 IER = 0x0000;
 IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2833x_DefaultIsr.c.
// This function is found in DSP2833x_PieVect.c.
 InitPieVectTable();
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
 EALLOW; // This is needed to write to EALLOW protected register
 PieVectTable.ADCINT = &adc_isr;
 EDIS; // This is needed to disable write to EALLOW protected registers
// Step 4. Initialize all the Device Peripherals:
// This function is found in DSP2833x_InitPeripherals.c
// InitPeripherals(); // Not required for this example
 InitAdc(); // For this example, init the ADC
// Step 5. User specific code, enable interrupts:
// Enable ADCINT in PIE
 PieCtrlRegs.PIEIER1.bit.INTx6 = 1;
 IER |= M_INT1; // Enable CPU Interrupt 1
 EINT; // Enable Global interrupt INTM
 ERTM; // Enable Global realtime interrupt DBGM
LoopCount = 0;
 ConversionCount = 0;
// Configure ADC
 AdcRegs.ADCMAXCONV.all = 0x0001; // Setup 2 conv's on SEQ1
 AdcRegs.ADCCHSELSEQ1.bit.CONV00 = 0x0; // Setup ADCINA0 as 1st SEQ1 conv.
 AdcRegs.ADCCHSELSEQ1.bit.CONV01 = 0x1; // Setup ADCINA1 as 2nd SEQ1 conv.
 AdcRegs.ADCTRL2.bit.EPWM_SOCA_SEQ1 = 1;// Enable SOCA from ePWM to start SEQ1
 AdcRegs.ADCTRL2.bit.INT_ENA_SEQ1 = 1; // Enable SEQ1 interrupt (every EOS)
// Assumes ePWM1 clock is already enabled in InitSysCtrl();
 EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
 EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
 EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
 EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
 EPwm1Regs.TBPRD = 400; // Set period for ePWM1
 EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start
// Wait for ADC interrupt
 for(;;)
 {
 LoopCount++;
 }
}
interrupt void adc_isr(void)
{
Voltage1[ConversionCount] = AdcRegs.ADCRESULT0 >>4;
 Voltage2[ConversionCount] = AdcRegs.ADCRESULT1 >>4;
// If 40 conversions have been logged, start over
 if(ConversionCount == 1499)
 {
 ConversionCount = 0;
 }
 else ConversionCount++;
// Reinitialize for next ADC sequence
 AdcRegs.ADCTRL2.bit.RST_SEQ1 = 1; // Reset SEQ1
 AdcRegs.ADCST.bit.INT_SEQ1_CLR = 1; // Clear INT SEQ1 bit
 PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}