We're confused about the jumper/switch settings on LaunchPAD-XL. What settings are needed to do Motorware labs with LaunchPAD-XL F28069M and BoostXL-DRV8301?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We're confused about the jumper/switch settings on LaunchPAD-XL. What settings are needed to do Motorware labs with LaunchPAD-XL F28069M and BoostXL-DRV8301?
from:
C:\ti\motorware\motorware_1_01_00_15\docs\boards\kits\docs\readmefirst_instaspin_launchboost.pdf
LAUNCHXL-F28069M
i. Remove Jumpers 1 and 2 to isolate USB and power from BOOSTXL-DRV8301
ii. S1 set to ON-ON-ON
iii. JP3, 6, 7 ON
iv. JP4, 5
a. ON-ON: if just using bottom BoosterPack headers J5-J8
b. OPEN-OPEN: if using top BoosterPack headers J1-J4 or using both BoosterPack headers J1-J4 & J5-J8;
c. Provide DC bus at any attached BoosterPack
Thank you. This helped immensely. With the jumpers and switches set as above, we were finally able to program the device and identify and run our motor.