Dear All,
We are facing problems related to dynamic range and resolution of 2P2Z controller. Using the standard 2P2Z controller we cannot reach enough dynamic range neither resolution, because we need a high dynamic range and high resolution at the same time, and it isn't possible using the standard solution. We tried to improve the dynamic range change from iq26 to iq19 but it was not enough to solve the dynamic range problem and brought low resolution problem (we need the iq26 resolution and iq16 dynamic range). Do you have any suggestion to implement this combination (iq26 resolution and iq16 dynamic range)? Do you have 2P2Z controller that works with 64 bit result of multiply operation instead of 32 bit result?
Thanks,
RR.