Other Parts Discussed in Thread: CODECOMPOSER
I have started a CAN communication project using board:
"TMS320F2812PGFA / CG-72AJF3W / G4" and DMC Developer Pro Software.
Now i have the board connected to my PC, also i have it powered and also
connected to a CAN bus with other CAN modules.
At my first steps i have loaded the demo can sample software to processor
RAM and all things worked great, that means that i have realized a can
communication within my CAN network (send and receive also).
Then, using Code Composer Studio and Flash Programmer Software
TMS320LF2812 i have written my test software into the processor FLASH
memory.
Now i noticed that the LED from the board is not ON anymore plus that i can
not connect to the board using monitor or other DMC software.
I'm not using a JTAG connector.
Can you send to me the default FLASH software?, or help with this issue?
Thank you.