Sorry I did not attach have a picture, and I probably will later, but I have a problem with the fitment of the BoostXL-Drv8301 and the LaunchpadXl_F28027F board. The 2 devices mate together, but the inserted length of the mating contacts do not allow a reliable fit. It looks like, the connector tail length of the LaunchpadXl-F28027F board is not long enough. When I connect the boards together, if I move the BoostXl-Drv8301 board, there is a 50% chance the boards will separate. The jumper switch height causes the booster pack to bottom out without making a physically reliable connection.
If I plug the BoostXL-Drv8301 into my old LaunchpadXl-F28027 board that is 2 -3 years old, and only has male headers top and bottom, the board has a very nice fitment, but then I do not have the FAST processor for InstaSpin
Is anyone else having this problem? I received the parts from the TI e-store this week.
I really like the time TI has put into this product, and I have a very soft spot in my heart for TI, but not being able to install CCSv6 Linux_64 and not having a reliable way to develop this system could be a deal breaker. I dusted off my old laptop (MSWIN JUNK) to install CCSv6, but I still need a reliable way to prototype; my environment is not that ideal