I am unable to program m3 and c28 into the F28M35
I am using a +15V lab supply and CCS V5.3.
I get to "Target -> Load Program" section and it goes from "Suspended" to "Running" but never finishes.
Here is what the CCS TI Window Explorer says when I try to "Target -> Load Program":
Cortex_M3_0: GEL Output: Memory Map Initialization Complete
Cortex_M3_0: Error connecting to the target: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.872.0)
Cortex_M3_0: GEL Output: Watchdog Timers Enabled
Cortex_M3_0: GEL Output: UARTs Enabled
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: Trouble Writing Memory Block at 0x4922 on Page 1 of Length 0x2: (Error -1141 @ 0x0) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.872.0)
C28xx_0: GEL Output:
RAM Initialization Complete
Cortex_M3_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Cortex_M3_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x204ef0: (Error -1066 @ 0x204EF0) Unable to set requested breakpoint in memory. Verify that the breakpoint address is in writable memory. (Emulation package 5.0.872.0)
Cortex_M3_0: Trouble Setting Breakpoint with the Action "Terminate Program Execution" at 0x206d78: (Error -1066 @ 0x206D78) Unable to set requested breakpoint in memory. Verify that the breakpoint address is in writable memory. (Emulation package 5.0.872.0)
C28xx_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.