Hi everybody
I have the TMS320F2812 DSP and I would like to program my board with the CCS 3.1. When I tried to "connect" i had the following error message:
Error connecting to the target:
Error 0x80000200/-2092
Fatal Error during: OCS,
Device driver: Emulation Connection Loss Detected on Target CPU.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
Sequence ID: 0
Error Code: -2092
Error Class: 0x80000200
I/O Port = 378
Board Name: F2812 eZdsp
Cpu Name: cpu_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
As if I haven't connected anything to my PC.
My PC (windows xp sp3) use a pci parallel port, just like that: http://www.comm5.com.br/2P-PCI-SLIM--2-SA%C3%8DDAS-PARALELAS#
I installed the drivers from parallel port, and nothing changed. I checked the setup and everything is ok, even the port adress (currently is set to 0x378, but i already tried all i/o availabe)
I don't know what i can do for solve this, so anyone can help me?