Hi,
we use the (modified by Trey German) USB bootloader for F28069U and also call it from our application using AppUpdaterUSB(). This has been working well so far, but we added a larger portion of code recently and problems started:
When we call the bootloader from the app now, the bootloader is entered/running as before (we indicate this by a LED), but the device gets reset within 500 ms or so. I could debug this a bit and found out that in the bootloader, HandleReset() in bl_usb.c is called, probably from a USB reset condition on the bus. Now I modified this function to not reset the device and the bootloader keeps running, but it is unusable/slow/... Sporadically it can be enumerated by "dfuprog -e", but only a single time and then the values printed out by dfuprog look really strange.
This is not a watchdog issue, as we disable the WD (verified) before we enter AppUpdaterUSB().
The code modifications we added in contrast to the working state before do not touch the bootloader or the application and its code for entering the bootloader at all, as far as I can tell. There are even no "new" interrupts or side-effects etc.
The only difference I can see right now is that we have "more code", i. e. more flash consumption... Can this be the source of the problem somehow?
What is the latest USB bootloader for F28069U, where can I find it, and does it also contain all the patches from Trey?
Help would be greatly appreciated, as we need a working bootloader for field upgrades also.
Felix