This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difference between F28069F and F28069



Hi all,

        I have piccolo controller with Instaspin-FOC enabled libraries in its Boot-ROM. I wanted to use it for a different application apart from Motor control. So when i checked the INSTASPIN-TRM ( SPRUHI9 ) , in page 21 they have mentioned that only 14 pwm's are available in 100-pin version of F28069F which contradicts with another table from the same document showing 16 pwm channels are available.

         Can anyone clarify on this. Also specify any hardware limitations with INSTASPIN enabled version.

Note: I will use linker command file of F28069 and i wont call any functions from the library.