Hi, i wonder if there is any experience in measurement of high precision high speed encoder signals using the eqep (for example 28335)? i'm using an encoder that is able to generate 3072 lines per rev and i'm trying to measure up to 18000rpm... this would result in a pulse train of 3.7Mhz after the quadrature sense.. is the QCLK in the eqep unit to capture the pulse train? the eqep doc
does not seem to have a direct information on the QCLK itself in the illustrations...
thanks