Hi
We are working on the ADC reference section of TMS320F28377DWT and we are sampling the input signal at 1MSPS rate (16-bit ADC)
We are using Ref3230 IC as the reference IC. and is connected to LMP7709MT op-amp which is configured as non-inverting buffer . It is connected to the Vref pin of ADC with the 22uF as suggested in DS of TMS320F28377DWT.
The DS of LMP7709 doesn't mention about the max capacitive load. Is it feasible to use LMP7709 as buffer IC ?