This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28x Issue Resolved: Stdout window disappears, Printf()'s, Fopen's, etc... do not work



Here is an issue that was recently resolved on a F28x device

The engineer had an existing *.out file that worked on co-worker's system.  This program made use of Printf()'s to the Stdout window as well as file accesses via fopen().  If the out file was loaded on the system in question, the stdout window was not even present and the fopen/fread did not access a file...

The root cause of the issue was due to CCS settings. 

When debugging from Flash on C28x (or TMS470) devices, there are only 2 HW breakpoints available.  By default, CCS uses two breakpoints, one for CIO accesses and another for end of program at load.  Typically, C28x users will go into CCS options to disable these breakpoints, thus maximizing the number of HW breakpoints available for debug out of flash.  However, if C I/O functions are used (printf, etc), and the CIO breakpoint is removed, the CIO functions will not work...

To resolve the issue

In CCS3.x

Go to Option->Customize->Program/Project/CIO

Under program load, make sure that "Do Not Set CIO Breakpoint At Load" is unchecked...

In CCS4.x

During debug session

Tools->Debugger Options->Generic Debugger Options

Under program/Memory Load options, make sure that "Enable CIO function use" is checked