This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PICCOLO f28027 controlstick Sci transmit program

I try to use Example_2802x0Sci_Echoback.c  to transmit TXD[6] ={0xff,0x55,0x01,0x0fe,0x00,0xff};  to other device 

I use one USB port to recevice the data 29 pin(TX)  ,but just InitSysCtrl(); work ,  pin 29 will send many data to PC USB port .

I can't send TXD[6] ={0xff,0x55,0x01,0x0fe,0x00,0xff};   to  PC

my code :

#include "DSP28x_Project.h" // Device Headerfile and Examples Include File

// Prototype statements for functions found within this file.
void scia_echoback_init(void);
void scia_fifo_init(void);
void scia_xmit(unsigned char a);
void scia_msg();//(char *msg);

// Global counts used in this example
uint16_t LoopCount;
uint16_t ErrorCount;


void main(void)
{
Uint16 ReceivedChar;
char *msg;
char *table;

// WARNING: Always ensure you call memcpy before running any functions from RAM
// InitSysCtrl includes a call to a RAM based function and without a call to
// memcpy first, the processor will go "into the weeds"
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif

// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the f2802x0_SysCtrl.c file.
InitSysCtrl();

// Step 2. Initialize GPIO:
// This example function is found in the f2802x0_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//InitGpio(); //Skipped for this example

// For this example, only init the pins for the SCI-A port.
// This function is found in the f2802x0_Sci.c file.
InitSciaGpio();

// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;

// Initialize PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the f2802x0_PieCtrl.c file.
InitPieCtrl();

// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;

// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in f2802x0_DefaultIsr.c.
// This function is found in f2802x0_PieVect.c.
InitPieVectTable();

// Step 4. Initialize all the Device Peripherals:
// Not required for this example

// Step 5. User specific code:

LoopCount = 0;
ErrorCount = 0;

scia_fifo_init(); // Initialize the SCI FIFO
scia_echoback_init(); // Initialize SCI for echoback

//msg = "\r\n\n\nHello World!\0";
//scia_msg(msg);

//msg = "\r\nYou will enter a character, and the DSP will echo it back! \n\0";
//scia_msg(msg);
//int i=0;
for(;;)
{
//able = "\r\nEnter a character: \0";
scia_msg();//(msg);

// Wait for inc character
//while(SciaRegs.SCIFFRX.bit.RXFFST !=1) { } // wait for XRDY =1 for empty state

// Get character
//ReceivedChar = SciaRegs.SCIRXBUF.all;

// Echo character back
//msg = " You sent: \0";
//scia_msg(msg);
//scia_xmit(ReceivedChar);

//LoopCount++;
}
}

// Test 1,SCIA DLB, 8-bit word, baud rate 0x000F, default, 1 STOP bit, no parity
void scia_echoback_init()
{
// Note: Clocks were turned on to the SCIA peripheral
// in the InitSysCtrl() function

SciaRegs.SCICCR.all =0x0007; // 1 stop bit, No loopback
// No parity,8 char bits,
// async mode, idle-line protocol
SciaRegs.SCICTL1.all =0x0003; // enable TX, RX, internal SCICLK,
// Disable RX ERR, SLEEP, TXWAKE
SciaRegs.SCICTL2.all =0x0003;
SciaRegs.SCICTL2.bit.TXINTENA =1;
SciaRegs.SCICTL2.bit.RXBKINTENA =1;
SciaRegs.SCICTL1.bit.TXENA = 1;
SciaRegs.SCICTL1.bit.SWRESET = 1;
// SCI BRR = LSPCLK/(SCI BAUDx8) - 1
#if (CPU_FRQ_60MHZ)
SciaRegs.SCIHBAUD =0x0000; // 9600 baud @LSPCLK = 15MHz (60 MHz SYSCLK).
SciaRegs.SCILBAUD =0x00C2;
#elif (CPU_FRQ_50MHZ)
SciaRegs.SCIHBAUD =0x0000; // 9600 baud @LSPCLK = 12.5 MHz (50 MHz SYSCLK)
SciaRegs.SCILBAUD =0x00A1;
#elif (CPU_FRQ_40MHZ)
SciaRegs.SCIHBAUD =0x0000; // 9600 baud @LSPCLK = 10MHz (40 MHz SYSCLK).
SciaRegs.SCILBAUD =0x0081;
#endif

SciaRegs.SCICTL1.all =0x0023; // Relinquish SCI from Reset
}

// Transmit a character from the SCI
void scia_xmit(unsigned char a)
{
while (SciaRegs.SCIFFTX.bit.TXFFST != 0) {}
SciaRegs.SCITXBUF=a;
//while (!SciaRegs.SCICTL2.bit.TXEMPTY) {}

}

void scia_msg()//(char * msg)
{
unsigned char TXD[6] ={0xff,0x55,0x01,0x0fe,0x00,0xff};
//unsigned char TXD[6]={1,2,3,4,5,6};
int i;
//i = 0;
//while(msg[i] != '\0')

for (i=0;i<6;i++)
{
scia_xmit(TXD[i]);
//i++;
}
}

// Initialize the SCI FIFO
void scia_fifo_init()
{
SciaRegs.SCIFFTX.all=0xE040;
SciaRegs.SCIFFRX.all=0x2044;
SciaRegs.SCIFFCT.all=0x0;
}

//===========================================================================
// No more.
//===========================================================================

any help ?  or can work's sample code  pls