Hello,
I am currently trying to use the CLA on the F28069 control card. I wish to have the initialized sections of memory loaded to flash and then copied over to ram for execution. I have successfully done this using a modified linker file and adding the copy section routine to my source code. As long as I do not use the CLA, everything copies over and works fine.
Using the CLA while programming and running from RAM seems to work fine as well. Its combining the two things that gives rise to problems.
When I try to use the CLA (with the copy sections routine). it behaves unpredictably. Sometimes the code will run (minus the CLA working) and other times my code will mange to fall into the illegal interrupt service routine. I have even seen the code not follow itself properly. (jump into the wrong function while stepping through the code). I added to the copysections routine to have it take care of the CLA program space. I also tried using memcpy in the CLA initialization and still have had no luck.
Here is the code I added to the Copy Sections routine.
I noticed that the debugger gives me this error when I try to read any variables that are stored in CLA memory space.
I think it might be my linker file. I dont get any errors when I compile my code however various linker files seem to give me different results. I also looked at the memory .GEL file and everything looks as it should.
I have attached the Linker file I am using. It is modified from the one included in control suite (for CLA with FLASH).
/*
//###########################################################################
//
// FILE: 28069_RAM_CLA_C_lnk.cmd
//
// TITLE: Linker Command File For F28069 examples that run out of RAM
//
// This ONLY includes all SARAM blocks on the F28069 device.
// This does not include flash or OTP.
//
// Keep in mind that L0,L1,L2,L3 and L4 are protected by the code
// security module.
//
// What this means is in most cases you will want to move to
// another memory map file which has more memory defined.
//
//###########################################################################
// $TI Release: F2806x C/C++ Header Files and Peripheral Examples V150 $
// $Release Date: June 16, 2015 $
// $Copyright: Copyright (C) 2011-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
*/
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\F2806x_headers\cmd
//
// For BIOS applications add: F2806x_Headers_BIOS.cmd
// For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd
========================================================= */
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */
/* Uncomment this line to include file only for non-BIOS applications */
/* -l F2806x_Headers_nonBIOS.cmd */
/* Uncomment this line to include file only for BIOS applications */
/* -l F2806x_Headers_BIOS.cmd */
/* 2) In your project add the path to <base>\F2806x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */
/* Define the memory block start/length for the F2806x
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F28069 are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
Contiguous SARAM memory blocks can be combined
if required to create a larger memory block.
*/
_Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x400
-stack 0x400
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
BEGIN : origin = 0x3F7FF6, length = 0x000002 //start at flash and not RAM.
RAML5L8 : origin = 0x00C000, length = 0x006000
RAML8 : origin = 0x012000, length = 0x002000
FLASH_AB : origin = 0x3F0000, length = 0x007F80 /* on-chip FLASH */
/* RAML0_L2 : origin = 0x008000, length = 0x001000 */
RAML3 : origin = 0x009000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* FPU Tables in Boot ROM */
FPUTABLES : origin = 0x3FD860, length = 0x0006A0
/* IQ Math Tables in Boot ROM */
IQTABLES : origin = 0x3FDF00, length = 0x000B50
IQTABLES2 : origin = 0x3FEA50, length = 0x00008C
IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA
BOOTROM : origin = 0x3FF3B0, length = 0x000C10
//PAGE 1 :
/* Part of M0, BOOT rom will use this for stack */
BOOT_RSVD : origin = 0x000002, length = 0x00004E
/* on-chip RAM block M1 */
RAMM0 : origin = 0x000050, length = 0x000400
RAMM1 : origin = 0x000480, length = 0x000380
CLARAM0 : origin = 0x008800, length = 0x000400
CLARAM1 : origin = 0x008C00, length = 0x000400
CLARAM2 : origin = 0x008000, length = 0x000800
/* on-chip RAM block L4-L8 */
RAML4 : origin = 0x00A000, length = 0x002000
/* RAML5 : origin = 0x00C000, length = 0x002000 */
/* RAML6 : origin = 0x00E000, length = 0x002000 */
/* RAML7 : origin = 0x010000, length = 0x002000 */
/* RAML8 : origin = 0x012000, length = 0x002000 */
FLASH_CD : origin = 0x3E8000, length = 0x008000 /* on-chip FLASH */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
}
SECTIONS
{
/*** User Defined Sections ***/
codestart : > BEGIN, PAGE = 0 /* Used by file CodeStartBranch.asm */
wddisable : > FLASH_AB, PAGE = 0 /* Used by file CodeStartBranch.asm */
copysections : > FLASH_AB, PAGE = 0 /* Used by file SectionCopy.asm */
ramfuncs : > RAMM1, PAGE = 0
// .text : > RAML5L8, PAGE = 0
// .cinit : > RAMM0, PAGE = 0
// .pinit : > RAMM0, PAGE = 0
// .switch : > RAMM0, PAGE = 0
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
.stack : > RAMM0, PAGE = 0
.ebss : > RAML4, PAGE = 0
// .econst : > RAML4, PAGE = 0
.esysmem : > RAML4, PAGE = 0
.sysmem : > RAML4, PAGE = 0
.cio : > RAML4, PAGE = 0
.scratchpad : > CLARAM0, PAGE = 0
.bss_cla : > CLARAM0, PAGE = 0
.const_cla : > CLARAM0, PAGE = 0
IQmath : > RAML4, PAGE = 0
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Allocate FPU math areas: */
FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD
.cinit : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */
RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */
LOAD_START(_cinit_loadstart),
RUN_START(_cinit_runstart),
SIZE(_cinit_size)
.const : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */
RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */
LOAD_START(_const_loadstart),
RUN_START(_const_runstart),
SIZE(_const_size)
.econst : LOAD = FLASH_CD, PAGE = 0 /* Load section to Flash */
RUN = RAML4, PAGE = 0 /* Run section from RAM */
LOAD_START(_econst_loadstart),
RUN_START(_econst_runstart),
SIZE(_econst_size)
.pinit : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */
RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */
LOAD_START(_pinit_loadstart),
RUN_START(_pinit_runstart),
SIZE(_pinit_size)
.switch : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */
RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */
LOAD_START(_switch_loadstart),
RUN_START(_switch_runstart),
SIZE(_switch_size)
.text : LOAD = FLASH_AB, PAGE = 0 /* Load section to Flash */
RUN = RAML5L8 , PAGE = 0 /* Run section from RAM */
LOAD_START(_text_loadstart),
RUN_START(_text_runstart),
SIZE(_text_size)
Cla1Prog : LOAD = FLASH_CD, PAGE = 0
RUN = RAML8, PAGE = 0
LOAD_START(_Cla1funcsLoadStart),
LOAD_END(_Cla1funcsLoadEnd),
RUN_START(_Cla1funcsRunStart),
LOAD_SIZE(_Cla1funcsLoadSize)
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 0
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 0
Cla1DataRam0 : > CLARAM0, PAGE = 0
Cla1DataRam1 : > CLARAM1, PAGE = 0
Cla1DataRam2 : > CLARAM2, PAGE = 0
CLA1mathTables : > CLARAM1,
LOAD_START(_Cla1mathTablesLoadStart),
LOAD_END(_Cla1mathTablesLoadEnd),
LOAD_SIZE(_Cla1mathTablesLoadSize),
RUN_START(_Cla1mathTablesRunStart),
PAGE = 0
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > CLARAM0,
PAGE = 0
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Thanks for you time and help,
Matt