This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

A problem about the function printf in F28377D project.



While I used F28377D chip and create a new project following the 'F2837xD Fireware Development Package user's guide' in CPU2. There is correct as the guide, but when I add the printf function for debugging the project, it will be a error as:

"../2837xD_RAM_lnk_cpu2.cmd", line 37: error #10099-D: program will not fit into available memory.  placement with alignment/blocking fails for section ".text" size 0x1cac page 0.

If I creat the project as a base project as hello wrold, and use the same *.cmd file, there is no error.

Where is the problem?