Other Parts Discussed in Thread: LAUNCHXL-F28027
Hello!
I want to connect C2000 Piccolo LAUNCHXL-F28027 and LCD 1602A. And I already found this example: embedjournal.com/.../. I downloaded the source code and connected pins as shown in the example, after that I used exactly the same code:
#define RS GPIO_Number_12
#define E GPIO_Number_19
#define D0 GPIO_Number_0
#define D1 GPIO_Number_1
#define D2 GPIO_Number_2
#define D3 GPIO_Number_3
#define D4 GPIO_Number_4
#define D5 GPIO_Number_5
#define D6 GPIO_Number_16
#define D7 GPIO_Number_17
GPIO_Handle myGpio;
/* Initializes LCD */
void InitializeLCD(void)
{
GPIO_setHigh(myGpio, E);
LCDDelay1600();
LCDDelay1600();
LCDDelay1600();
LCDDelay1600();
WriteCommandLCD(0x38); //Command to select 8 bit interface
LCDDelay1600();
WriteCommandLCD(0x38); //Command to select 8 bit interface
LCDDelay(); //Small delay
WriteCommandLCD(0x38); //Command to select 8 bit interface
LCDDelay();
WriteCommandLCD(0x08); //Command to off cursor,display off
WriteCommandLCD(0x01); //Command to Clear LCD
LCDDelay1600();
WriteCommandLCD(0x06); //Command for setting entry mode
WriteCommandLCD(0x0f); //Command to on cursor,blink cursor
WriteCommandLCD(0x02); //Command return the cursor to home
LCDDelay1600();
DisplayLCD(1, "hello");
}
/* Writes a command byte to LCD */
void WriteCommandLCD(unsigned char CommandByte)
{
GPIO_setLow(myGpio, RS); //Clear RS pin to write command
SendByte(CommandByte);
LCDDelay(); //Small delay
}
/* Send a byte of data to LCD */
void SendByte(unsigned char Value)
{
unsigned char temp;
if((Value & 0x01) == 0x01)
GPIO_setHigh(myGpio, D0);
else
GPIO_setLow(myGpio, D0);
if((Value & 0x02) == 0x02)
GPIO_setHigh(myGpio, D1);
else
GPIO_setLow(myGpio, D1);
if((Value & 0x04) == 0x04)
GPIO_setHigh(myGpio, D2);
else
GPIO_setLow(myGpio, D2);
if((Value & 0x08) == 0x08)
GPIO_setHigh(myGpio, D3);
else
GPIO_setLow(myGpio, D3);
if((Value & 0x10) == 0x10)
GPIO_setHigh(myGpio, D4);
else
GPIO_setLow(myGpio, D4);
if((Value & 0x20) == 0x20)
GPIO_setHigh(myGpio, D5);
else
GPIO_setLow(myGpio, D5);
if((Value & 0x40) == 0x40)
GPIO_setHigh(myGpio, D6);
else
GPIO_setLow(myGpio, D6);
if((Value & 0x80) == 0x80)
GPIO_setHigh(myGpio, D7);
else
GPIO_setLow(myGpio, D7);
GPIO_setHigh(myGpio, E); //Set E pin to select LCD
for(temp=0;temp<5; temp++);
GPIO_setLow(myGpio, E); //Clear E pin to deselect LCD
LCDDelay(); //Small delay
}
/* Writes a Data byte to LCD */
void WriteDataLCD(unsigned char DataByte)
{
GPIO_setHigh(myGpio, RS); //Set RS pin to 1 to write Data
SendByte(DataByte);
LCDDelay(); //Small delay
}
/* Small delay */
void LCDDelay(void)
{
DELAY_US(500);
}
/* Big delay */
void LCDDelay1600(void)
{
DELAY_US(16000);
}
/* Makes cursor visible */
void CursorON(void)
{
WriteCommandLCD(0x0f); //Command to switch on cursor
}
/* Makes cursor invisible */
void CursorOFF(void)
{
WriteCommandLCD(0x0c); //Command to switch off cursor
}
/* Displays a message on LCD */
void DisplayLCD(char LineNumber,char *Message)
{
int a;
if(LineNumber ==1)
{ //First Line
WriteCommandLCD(0x80); //Select the first line
}
else
{ //Second line
WriteCommandLCD(0xc0); //Select the second line
}
for(a=0;a<16;a++)
{
WriteDataLCD(*Message); //Display a character
Message++; //Increment pointer
}
return;
}
void main(){
InitializeLCD();
}
But after execution of this code absolutely nothing has changed on the LCD - I see only a several rectangles in the first line(just like the after power up). I think that is because lm016l used in the example, but I use 1602A. Could it be? If yes then which functions I need to change and how exactly I need to change them? Please give me comprehensive information if you can, because I am a novice at this and it's very hard to understand what I exactly need.
Thanks!