This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reliable driver kit?

Other Parts Discussed in Thread: DRV8301, LAUNCHXL-F28027F, MOTORWARE, LAUNCHXL-F28069M, BOOSTXL-DRV8305EVM

I am looking for driver kit to drive a BLDC motor. The basic feature that I need are, the kit should operated upto 36V, 10A. Please suggest me a driver or a driver with booster pack. Actually I am looking or a driver that will fit into my budget. I had a practice on drv8301 piccolo f28027 with booster pack. Can i use this for the above ratings. Please suggest. 

Thank you.

  • I would suggest BOOSTXL-DRV8305EVM which you can pair with LAUNCHXL-F28027F or LAUNCHXL-F28069M (SW support for combination with 69M will be included in next version of MotorWare end of February).

    alternatively you could use DRV8301-69M-KIT which is fully supported now. It is just much larger, more expensive, and the voltage and current scaling are higher than you require, so you will lose a bit of performance due to signal resolution.