Hello
I am implenting a three phase inverter. I am using IPM (Intelligent power module) for this purpose.
I designed an optocupler circuit to isolate the IPM and ezdsp 320f2812 kit. There is an alarm output on IPM for warning the under voltage, overvoltage and high temperature. I want to take this alarm information into DSP. The diode side voltage of the optocupler(VCC_IPM) is from IPM and for the transistor side voltage of the optocoupler I designed a 3.3 V output voltage regulator (ALM_3.3V and ALMGND).
I want to ask these:
1 - Will I use GPIO to take this alarm information into DSP?
2- If I use this pin or other, must I conncet the GND of the DSP with tranasistor side GND of optocoupler (ALMGND) ? If I have to do this I will have connected the GND of 15 V supply voltage of 3.3 V regulator with the DSP GND. Won't be harmful for the DSP connecting the GND of 15 V supply with DSP GND?
I inserted the schematic of the opto circuit . Thank you all....