Hi,
What's the maximum SCI baud rate the can be used to communicate with the TI-PLC-G3-FCC-SN SOM in FCC mode? The older kits use 57600 but with the extra bandwidth available in FCC mode it'd be nice to be able to connect at 115200.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
What's the maximum SCI baud rate the can be used to communicate with the TI-PLC-G3-FCC-SN SOM in FCC mode? The older kits use 57600 but with the extra bandwidth available in FCC mode it'd be nice to be able to connect at 115200.
Thanks.
Hi Darryl,
Even for the TI-G3-FCC SN SOM the SCI baud rate is 57600.
Regards.