Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28377S -- eQEP Unable to Clear Capture Timer Overflow Error Flag

I am using the quadrature encoder module to measure position and estimate velocity of an encoder. To estimate velocity, I use the low-speed approximation, v(k) = X / (t(k) - t(k-1)), where X is unit position. To do so, I set the appropriate registers in EQep1Regs:

EQep1Regs.QCAPCTL.bit.UPPS = 0;		// UPEVNT = QCLK/1   (i.e. one tick)
EQep1Regs.QCAPCTL.bit.CCPS = 0x7;	// CAPCLK = SYSCLKOUT/128
EQep1Regs.QCAPCTL.bit.CEN = 1;		// Enable

along with other EQep1Regs not shown. For simplicity, I use register polling (instead of interrupts), to update my velocity estimation. Every loop cycle, I run:

if (EQep1Regs.QEPSTS.bit.UPEVNT == 1) {
	Uint16 delta_T = EQep1Regs.QCPRD;
	double dt = (((double) delta_T) / 200000000.0) * 128.0;	 // CAPCLK = SYSCLKOUT/128
	v_lo_speed = DX / dt; // DX is previously defined as a double unit length
	EQep1Regs.QEPSTS.bit.UPEVNT = 1;	// Reset UPEVNT flag
} else if (EQep1Regs.QEPSTS.bit.COEF == 1) {
	v_lo_speed = 0.0;
	EQep1Regs.QEPSTS.bit.COEF = 1;  // DOES NOT CLEAR COEF bit!
}

I've also tried using each and every QCLR bit to clear the COEF, as the technical reference manual (SPRUHX5C, pg 1855) instructs. However, there is no QCLR bit that corresponds to the QEPSTS.bit.COEF bit.

Which register should I use to clear the capture timer overflow error flag?

  • Hi Zachary,

    Looks like the documentation is incorrect. You need to write "1" COEF bit of QEPSTS to clear it.
    So, you are doing the right thing to clear the bit - EQep1Regs.QEPSTS.bit.COEF = 1;
    Can you check if it's getting set again, due to another overflow?
    can you step through the code and see the effect of clear?

    -Bharathi.
  • Yes, setting the EQep1Regs.QEPSTS.bit.COEF to 1 does indeed clear the bit. I wasn't seeing this before since I had set EQep1Regs.QEPCTL.bit.FREE_SOFT = 2, which keeps all the counters running while paused in debug mode. When I set EQep1Regs.QEPCTL.bit.FREE_SOFT = 0, I immediately see the effect of the clear. Most likely, when FREE_SOFT = 2, the counter overflows before I have time to see it being cleared.

    Thanks for your help.

    -Zach

  • Thanks. Good luck. will fix the documentation.