This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

delfino dual adc triggered with EPMW SOCA not work

Hello

I'm using delfino dual demo board

and I want to produce PWM out A&B waveforms

and acquire in a specific point of TB couter.

My code is

	EALLOW;

		CpuSysRegs.PCLKCR2.bit.EPWM1	= 1;

		EPwm1Regs.TBCTL.bit.PRDLD		= TB_SHADOW;
		EPwm1Regs.TBCTL.bit.CTRMODE		= TB_COUNT_UPDOWN;
		EPwm1Regs.AQCTLA.bit.CAD		= AQ_SET;
		EPwm1Regs.AQCTLA.bit.CAU		= AQ_CLEAR;
		EPwm1Regs.DBCTL.bit.OUT_MODE	= DB_FULL_ENABLE;
		EPwm1Regs.DBCTL.bit.POLSEL		= DB_ACTV_HIC;
		EPwm1Regs.TBPRD					= TBPRD;
		EPwm1Regs.CMPA.bit.CMPA			= TBPRD/2;

		// controllo SOCx, p1533 di SPRUHM8B–December 2013–Revised August 2014

		EPwm1Regs.ETSEL.bit.SOCAEN		= 1;
		EPwm1Regs.ETSEL.bit.SOCASEL		= ET_CTR_PRD;
		EPwm1Regs.ETSEL.bit.SOCBEN		= 1;
		EPwm1Regs.ETSEL.bit.SOCBSEL		= ET_CTR_ZERO;

		// controllo out MUX

		GpioCtrlRegs.GPAPUD.bit.GPIO0	= 1;			// Disable pull-up on GPIOx
		GpioCtrlRegs.GPAMUX1.bit.GPIO0	= 1;			// Configure GPIOx as EPWM

		GpioCtrlRegs.GPAPUD.bit.GPIO1	= 1;			// Disable pull-up on GPIOx
		GpioCtrlRegs.GPAMUX1.bit.GPIO1	= 1;			// Configure GPIOx as EPWM

    EDIS;

for the EPWM, and for the ADC I select TRIGxSEL 5&6 (ePWM1, ADCSOCA/C & ePWM1, ADCSOCB/D)

but ADC doesn't start acquire.

Can someone Help me?

Thank you