Other Parts Discussed in Thread: CONTROLSUITE
Hello everyone,
I am planning to develop a PCB with a F28335 microcontroller. To be able to program it, i would like to use a USB-JTAG-circuit on the board.
Examining the "USB Docking Station R3" schematic, I realized, that the pins EMU0 & EMU1 are just connected to the additional JTAG socket. Do I not need them for programming the µC ?
I also found the XDS100v2 schematic, which is more complex than the Docking Station circuit. I don't think, that I need the option to program a lot of different controllers (CPLD), as I just want to program the installed F28335. Increased speed would be a nice thing though. I guess it's not possible to take the v1 and just change the FT2232D to the FT2232H for higher speeds !?
What would be your suggestion ?
Thank you in advance.