Hi,
I want to use the I2C on the mircocontroller to receive data from an external ADC. From the control card schematic, it looks like the pins SDAA (GPIO_28) and SCLA (GPIO_29) are connected to FT2232H. Is there a way to use the I2C while still being able to program the control card using the USB ?
Thanks,
Prasanta.