This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CRC calculation with VCU2 on F28377S Launchpad

Hello everybody,

Im trying to calculate the CRC checksum of a frame with 19 bytes:

A8 01 08 2E E8  2E D0 2E F0 2E E0 2E  E0 2E E0 2E E0 2E E0


with the polynom 0x1021 and CCITT XMODEM. As result I expect 0x57B4.

However when I try to use the VCU2 library I never get this result. I already tried all combinations of odd/even and reflected, still no success...

Does somebofy know whats wrong with my code?

Thank you very much!

	const uint8_t testSUMD[] = 
	{
	 0xA8, 
	 0x01, 
	 0x08, 
	 0x2E, 0xE8, 
	 0x2E, 0xD0, 
	 0x2E, 0xF0, 
	 0x2E, 0xe0, 
	 0x2E, 0xE0, 
	 0x2E, 0xE0, 
	 0x2E, 0xE0, 
	 0x2E, 0xE0 
	};

CRC_Obj    CRC;

CRC_Handle handleCRC;

handleCRC = &CRC;


    CRC.seedValue    = 0;
    CRC.nMsgBytes    = 19;
    CRC.parity       = CRC_parity_odd;
    CRC.crcResult    = 0;
    CRC.pMsgBuffer   = (uint16_t *) &testSUMD[0];
    CRC.pCrcTable    = NULL;
    CRC.init         = (void (*)(void *))CRC_init16Bit;
    CRC.run          = (void (*)(void *))CRC_run16BitPoly2;

    CRC.init(handleCRC);
CRC.run(handleCRC);
int crc = CRC.crcResult;