While compling SPI example for LAUNCHXL-F28377S, I get the following error,... do anyone have idea about this problem...
<Linking>
warning #10210-D: creating ".esysmem" section with default size of 0x400; use the -heap option to change the default size
undefined first referenced
symbol in file
--------- ----------------
_SysCtrlRegs SPI\utility\c2000_spi.cpp.o
error #10234-D: unresolved symbols remain
warning #10063-D: entry-point symbol other than "_c_int00" specified: "code_start"
error #10010: errors encountered during linking; "BarometricPressureSensor.cpp.elf" not built
>> Compilation failure