Other Parts Discussed in Thread: MOTORWARE, DRV8301
Hi,
I've tried to spin my motor with the example project lab04a in torque mode. That works all fine, as I try to stop the motor, the current and the torque increase as well until the maximum current is reached (I set the maximum current to 15 amps in the user.h). But once the motor is decellerated until it stands still, the current drops to a maximum current of about 2.5 amps. This is also the case if I want to start the motor from 0rpm with a load that needs more torque than the 2.5 amps can generate.
Is there a way I can get more starting current (torque)? I've already tried out changing motor and controller parameters, as well as activating the ForceAngle checkbox, but that didn't help. Is there even a limitation of starting torque with a sensorless solution?
Thank you for any help in advance.
My hardware:
DRV8301-69M-KIT
C2000™ InstaSPIN™ TMS320F28069M MCU
Motorware_1_01_00_14