Hi,
I have problem with erasing TMS320F2802x device. I am using Flash_API erase function and I'm getting the error message 24 - Status Fail Precompact after Error function is calling. All other Flash_API functions works fine(verify or program), also toggle test is working...so I don't understand why erase function not. I am using the Flash API library "Flash2802x_API_V201.lib".
I found that debugging the erase function through CCS5v5 works fine. But after downloading code direct to RAM and run it from this location I get the error message 24 - Status Fail Precompact.
What is the reason of this error message?
Why erase function works during debugging but not in real application? Any ideas?
Thank you for your help!
Best regards,
Tomas