hi ;
I use motorware lab5b project , board is my own . when I download program , then enable" gMotorVars.Flag_enableSys" then enable "gMotorVars.Flag_Run_Identify"
js file immediately trun error .. but motor begin run . that mean Flag_Run_Identify can trig one time .
consol window show:
C28xx: Error: (Error -1135 @ 0x3F26C7) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.507.0)
C28xx: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0)
C28xx: Error: (Error -1135 @ 0x3F26C7) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.507.0)
C28xx: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.507.0)
C28xx: Error: (Error -1135 @ 0x3F26C7) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.507.0)
C28xx: Power Failure on Target CPU
where can I check . ?