This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debugger/Emulator for TMS320F28035



Hi, I am doing a microinverter project and cannot afford the more expensive XDS560v2 System Trace USB Debug Probe. I found the XDS100v2 JTAG Debug Probe but I need an adapter for it since it only has 14 pins instead of 56, but I can't find an adapter. Any other Debuggers around that price range that would work would also be great .

Thank you.

  • Hello Korben,

    What is it you are trying to do that would need to XDS560v2?  The C2000 family (e.g., F28035) does not have support for the system trace capability.  The recommended emulators for C2000 are XDS100v2 at the low-end, and XDS200 as a higher performance choice.  There is really nothing to be gained from an XDS560 class emulator with C2000.

    Also, where is the 56-pin connector coming from?

    Regards,

    David