Hi,
i see on board just to GPIO ports - GPIO60 and GPIO61. If I need more digital outputs from the board, in real-time, how can i do this? is there a possibility to use other pins on the board like ePWM, CAP, CAN as output ports for more GPIOs?
if not, i understand the only way to do so is to use one of the communication protocols. which one is recommended? if the needed frequency is about 100kHz?
Thanks in advance,
Israel