This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 CLA compiler issue

So, I'm getting started with the CLA co-processor and I'm running into a strange issue.

I've built a .cla file into an existing project.  But it doesn't seem to compile correctly in my project but it will in the sample project.

For instance:

Converting a long (stored in the CPU to CLA memory space).

float fTemp = 0;


__mdebugstop();

fTemp = 0;

fTemp = (float)xAdcInput;

tempF = tempF * 3.0;

xResult= (int)tempF;

In my program, the dis-assembly looks like this:

00009010: 78400000 MMOVIZ MR0, #0x0
00009012: 74C08C00 MMOV32 @0x8c00, MR0
00009014: 73C01506 MMOV32 MR0, @0x1506, UNCF
00009016: 74C08C00 MMOV32 @0x8c00, MR0

0000902a: 77804040 MMPYF32 MR0, #0x4040, MR0
0000902c: 74C08C00 MMOV32 @0x8c00, MR0

00009040: 7D600000 MF32TOI32 MR0, MR0
00009042: 74C01480 MMOV32 @0x1480, MR0

But in the example program (built from the fir32 example for the 28035 v1.30 ), the dis-assembly looks like the following:

0000900e:   74401500    MI32TOF32  MR0, @0x1500

00009028: 77804040 MMPYF32 MR0, #0x4040, MR0
0000902a: 7D600000 MF32TOI32 MR0, MR0
0000902c: 74C01480 MMOV32 @0x1480, MR0

Why is the same code different after compiling...  I've gone through the project... the compiler rev is the same (TI v6.4.9) the cla0 options are the same.

I don't get why this is happening.  What's wrong here?  Why isn't my project using the MI32TOF32 assembly among other issues?

Thank you,

Kyle