Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hi,
We are using drv8301 and motorware as a current source to do some test. The goal is to supply various frequency 3ph current. I notice that I can set the USER_ZEROSPEEDLIMIT at my desired frequency. I also need to set motor max current in user motor parameter to my desired current magnitude. So the code is always in the forced angle state.
It works at high frequency like >15Hz. I noticed at low frequency <10Hz. The current magnitude is a lot lower than the max current. Since I cannot see the forced angle code, I am not sure what happened. Is there anything I can do to increase the forced angle current at low frequency?
Yichao