Other Parts Discussed in Thread: TMDSCNCD28035, CONTROLSUITE
HI,
I'm using this equipment:
PC Dell Precision T3600, Windows7, F-Secure,
CCS Version: 6.1.0.00104
TMS320C2000 Experimenter Kit with Piccolo F2803x controlCARD, TMDSCNCD28035 R1.1
I'm using just a USB cable between PC and experimenter kit and I would like to start writing a simple test program. After "Test Connection" the reset command SW log seems to be OK, but the reset command HW log reports problems (see below and attachments) that I cannot resolve.
Many thanks in advance for any help.
Best regards,
Leo Rohrecker
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).
An error occurred while hard opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-150' (0xffffff6a).
The title is 'SC_ERR_FTDI_FAIL'.
The explanation is:
One of the FTDI driver functions used during
configuration returned a invalid status or an error.
[End: Texas Instruments XDS100v1 USB Debug Probe_0]