This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Difficulties with passing a character array to a function




My code calls a function that passes a boolean array and will return a character according to a global char array, depending on which boolean array value is 1. The code below is intended to a return a '2'. However when I add kp_keyPressed as a watch expression it shows that the value returns a '.' I'm not an expert dealing with arrays but from the code I've gone through online, my method of passing an array should work. Is there something weird about CCS that makes it so that this operation fails? Does the watch expressions table have some glitches when it comes to arrays? If the answers to those questions are no, is there something I'm doing wrong in the code below? Should I just steer clear of attempting to pass char arrays to functions? I am running the code on a 377S launchpad. Would appreciate any feedback. Thanks!

char KP_Key[16] = {"123A456B789C*0#D"};

Uint16 KP_Test[16] =
{
{0,1,0,0,
0,0,0,0,
0,0,0,0,
0,0,0,0}
};

char KP_FindKey(Uint16 array[16])
{
Uint16 i = 0;
char Key = 0;
for (i=0;i<16;i++)
{
if(array[i] == 1)
{
Key = KP_Key[i];
}
}
return Key;
}

void main()
{
char kp_keyPressed = KP_FindKey(KP_Test);
}



  • Benjamin,

    Look carefully at the way you have defined your array.  The double brackets on each end means it only has one element.  I think what you wanted was:

    Uint16 KP_Test[16] =
    {
    0,1,0,0,
    0,0,0,0,
    0,0,0,0,
    0,0,0,0
    };

    Also, define kp_keyPressed outside main, like this:

    char kp_keyPressed;

    main()
    {
    kp_keyPressed = KP_FindKey(KP_Test);

    }

    Then CCS should give you the answer you expect.

    Regards,

    Richard