Other Parts Discussed in Thread: CONTROLSUITE
Hi,
in the TMS320F2837xS Delfino™ Microcontrollers documentation (SPRS881B) I found a Chapter (cited below) about a CLB in the MCU. Is there some more Information about this CLB? Or is the CLB configuarble only for TI and not for the user?
I am missing a Technical Reference Manual for the 28379 (as e.g. available for the 28377), too.
Thanks
Frank
6.14 Configurable Logic Block (CLB)
The configurable logic block enables TI to offer additional interfacing and control features for select C2000
devices. TI utilizes the CLB to create specific on-chip solutions, such as Position Manager, that would
otherwise be accomplished using additional logic devices. Configuration files, application programmer’s
interface (API), and use examples are provided with the C2000 controlSUITE software package. In some
solutions, the TI-configured CLB is used in conjunction with other on-chip resources, such as the SPI port
or the C28x CPU, to perform more complex functionality. See Table 3-1 for the devices that support the
CLB feature.