This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

query about difference between PWM channels in F28335.

i am using f28335 experiment kit. i have configured ePWM2 for which voltage level is (3.4V for high), but when i configure ePWM1, voltage level for high is (3V). why this? Is there any difference between this two PWM channels? can voltage level drops due to frequent use of PWM pins of board?