This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMSM open loop

Other Parts Discussed in Thread: CONTROLSUITE

Hi,

I am testing EMJ -04 PB22 , 200Hz, 200V motor in open loop. 

I am planning to rotate the stator field at some 2000Hz. with a small magnitude

My intention is to check the effect on stator currents ia, ib, ic when the stator field crosses the rotor field and thus find the initial  position of the rotor

Is there a chance that the rotor gets locked to the stator field at this frequency. Or what freq and Vq, Vd can i apply to do this test.

Regards,

Dijo