Question (1)
We would like to output only one phase of ACIM PWM output at one time to help hardware problem validation during mass production. How to enable only one channel of PWM (eg.phase U), while disable 2 phases of PWM (eg.V and W disabled), the phase V and W PWM pins set to 1 or 0 which switch off MOSFET driver (we used IR2101S)
Question (2)
We found that sometimes, the motor under driving may lose synchronization when drive to extra high speed, and turn into high frequency vibrating instead of rotating as expected. We hope the software can detect such situation and restart the controller, is there any run-time variables can tell such situation happens ?
Thanks in advance.