This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK28027 docking station



Which is pin 1 and pin 2 (of the solder-able part of the docking station) so that I can figure out all pin allocations from control suite schematic). Please draw two arrows to indicate pin 1 and pin 2 in photo provided.

Regards,

Amit