Other Parts Discussed in Thread: CONTROLSUITE, SM320F28335-HT
I am using Pmsm3_4 code for speed control of pmsm motor with maximum speed rating of 4000 rpm. It seems to be working satisfactorily for speed commands of 200 rpm and above but when i try to go below 200 rpm the motion of the motor gets bumpy and it does not rotate smoothly. I have tried tuning the speed pid gains and the D and Q current pid gains as well but i still dont observe the required smooth motion.
Is the problem due to incorrect pid gains or something else? Is it required to generate high torque to rotate motor at low rpms?
I am required to run the motor at very low speed around 20 to 30 rpm.
Thank you.