HI,
How to calculate Vq testing value in PMSM FOC sensorless control open loop test ?
My motor is rated for 200V, 200Hz.
Does Vq Testing = 1 pu corresponds to 200*sqrt(2)/sqrt(3)= 163.3 V (conversion from line-line RMS value to peak phase value).
For increasing the voltage across the motor terminals do we need to increase the value of VdTesting. Or is it kept at zero only?
Regards,
Dijo