Other Parts Discussed in Thread: DRV8301
hi;
I am using;
tms320f28027f, c2000 launchpad with a maxon bldc motor and drv8301 motor drive.
I am trying to get the motor run as a generator whilst being driven by another motor.
My understanding of a BLDC motor would suggest that by simply driving the motor, I am already generating electricity.
However, I am looking at the schematic of the drv8301 motor drive, and I am seeing three of the six mosfets in the reverse direction.
My question is;
Am I supposed to control these MOSFET's in oder to produce a generator, or are they used for another purpose, such as allowing the motor to run in a reversed direction?
If they are used as part of a generator control system, can I be shown the direction towards the resources that will enable me to do this
Thanks