Hello,
Is there an oscillator frequency tolerance range requirement for the 28035 eCAN? There is section 21.13.1.4 of the 28075 TRM for instance which spells out the max "df" for DCAN (different part, different CAN), but I couldn't find a similar requirement in the eCAN guide or datasheet for 28035. I want to make sure the ceramic oscillator on the F28035 ISO ControlCard (CSTCE20M0V53-R0) is acceptable for using the eCAN, since it appears to marginally exceed the limits I derive using the 28075 TRM guideline, over temperature. It would be easier to know that the external oscillator is reliable to use instead of having to implement the oscillator temperature compensation approach, since my application is a real-time control loop and the ADC is already heavily utilized.
Thank you,
Dave