1) I used UniFlash (v3.4) to program both M3 and C28 with GUI and command-line.
UniFlash seems to erase the sectors, program and verify without any error.
2) But, when I erased the flash on both core first, performed a blank check.
Then program C28 and M3. Uniflash hanged, spinning....
What is the procedure for program a fresh (blank) F28M35x device using UniFlash?
Thanks.