Hello,
I would like information about the DRV8312-C2-KIT "Three Phase BLDC Motor Kit with DRV8312 and Piccolo MCU".
I need to know if the software demo provided allows you to run drills up to 40000 rpm in BLDC mode
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I would like information about the DRV8312-C2-KIT "Three Phase BLDC Motor Kit with DRV8312 and Piccolo MCU".
I need to know if the software demo provided allows you to run drills up to 40000 rpm in BLDC mode
Thank you
Our motors have the following features:
Motor1: R=2.13 Ohm L=120uH I=3.5A PolePairs=1
Motor2: R=2.43 Ohm L=145uH I=3.0A PolePairs=1
the required speed from 100 to 40000 rpm
it is possible for me to realize this application with your kit?
thank you
Hi Paolo,
It appears to be possible, although you may run into problems with the current limits of the DRV8312. The BOOSTXL-DRV8301 may be a better fit.
Please refer to LINK1 and LINK2 for tips.
In particular, note the comment in LINK2:
How low of inductance? You probably need to increase your PWM frequency significantly. Most low inductance BLDC speed controllers run at 60-72 KHz.
Do you know how much flux this motor has? Max current under load? Bus voltage?
You may want to consider using InstaSPIN-FOC or InstaSPIN-MOTION. You can simply use a different controlCARD with your DRV8312 board, but if you are using a <=24V bus or very low flux motors you will want to change the inverter hardware to BOOSTXL-DRV8301 and use LAUNCHXL-F28027Ffor the controller.
For instaSPIN questions, please post on the microcontroller C2000 forum.
Dear support, I am colleague of Paolo Colombari.
I have the TI DRV8312EVM Rev.D kit and CC2803x iso dimm.
I have programmed the InstaSPIN-BLDC_GUI_DRV8312_v104.out firmware and used the related application .
My motor have 1 pole pair, and in the setting TAB it isn't possible to select a 2 pole.
Anyway with InstaSPIN-BLDC_GUI_DRV83xx_v104.exe, I'm able to drive the motor up to a speed of approximately 30k rpm (displayed 15k )
How can I test the motor wih 2 pole and 40k rpm ?
How can I find the file source of InstaSPIN-BLDC_GUI_DRV8312_v104.out firmware ?
Thanks