Other Parts Discussed in Thread: TMDSCNCD28069, CONTROLSUITE, DRV8301
Hi,
I am using the Inverter DRV8301-HC-EVM Rev D together with the control card TMDSCNCD28069. I am using InstaSPIN-FOC for sensorless FOC. I am aware of the fact that sinusoidal commutation is superior to block commutation in most application cases. However, we need to fulfill this customer requirement.
Ideally, I would like to use the InstaSPIN Lab02b and extend it by the block commutation mode. It should be possible to switch between sensorless FOC and block commutation under load. Could anyone provide a code segment which covers the block commutation mode and elaborate briefly on how to integrate it into the existing control scheme?
Kind regards,
Oliver